This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Transmit/Receive simultaneously during EMC testing

Part Number: CC2640R2F

Good afternoon!

Our Bluetooth devices are currently undergoing EMC testing.  They are running the Host Test project for the original blestack (SDK 5.30.00.03).

For RX immunity testing, the test lab would prefer that the device transmit and receive during a single test scan.

Do either the Smart RF Studio tests (e.g., "Continuous TX", "Packet TX") or BTool tests (e.g., "HCIExt_ModemTestTxCmd", "HCI_LE_TransmitterTest") incorporate any bi-directional communication? (i.e., are handshake packets sent and received during the test?)

Thanks!

-Kenton