Part Number: CC2650
Other Parts Discussed in Thread: CC2630,
Hi team,
As title ask, is CC2650's private protocol file(.hex) compatible with CC2630?
BR
Sirui
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sirui,
The CC2630 is the same device as the CC2650 without BLE support. So long as their Prop RF solution does not use a BLE PHY and the packages are identical it could be possible to program a CC2630 with an image originally built for the CC2650. These parts have previously been shown to be binary compatible for IEEE and Zigbee applications.
Regards,
Ryan