This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P7: Reset Bond Manager NV

Part Number: CC2652P7

Hello.

On one devices I had a bug pairing do not work.

The connection work but pairing not stored and somme time device stop working.
If i check GAPBOND_BOND_COUNT he stay to 0.

I have try to execute one time GAPBondMgr_SetParameter(GAPBOND_ERASE_ALLBONDS,NULL); but that not fix the bug.

Finaly i erase full flash with jtag and now all work fine. pairing is store and GAPBOND_BOND_COUNT increas.
I think the NV use by GAPBondMgr was corrupt and i have fix it with a full flash erase, but it is not possible for the final user. Then i want to add the possibility to full erase / reset the NV of GAPBOND in code it is possible?