This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SubVersNr: 39445 - eSCO link not being requested by HF AG



I have a rather esoteric bug, I hope this is the right place for support.

I am trying to create an HFP audio link between a TI-powered infortainment system and a headset powered by Qualcomm QCC5127 

The only information I have about the TI chipset comes from the LMP_version_res packet, it contains this data

  • VersNr: Bluetooth Core Specification 4.2
  • CompId: Texas Instruments Inc.
  • SubVersNr: 39445 (0x15 0x9a)

I hope the TI engineers can back-trace the subversion number to the BT controller FW build.

The HFP service level connection seems to work OK, but the TI device never attempts to open any kind of eSCO link, which means there's no audio in the headset. 

Here is a trace of the HFP service level connection setup, if that helps

AT+BRSF=955. Retrieve AG Supported Features
..+BRSF: 2088.. Retrieved AG Supported Features
..OK.. Success
AT+CIND=?. Get supported indicators
..+CIND: ("service"(0-1))("call"(0-1))("callsetup"(0-3))("callheld"(0-2))("battchg"(0-5))("signal"(0-5))("roam"(0-1)).. Indicators supported
..OK.. Success
AT+CIND?. Get indicators' status
..+CIND: 1000550.. Indicators' status
..OK.. Success
AT+CMER=3 0 0 1. Enable "indicators' status reporting"
..OK.. Success
AT+OBISF=3. AT+OBISF=3
..+BSIR: 1.. The AG provides in-band ring tone
..ERROR.. Error
AT+VGS=08. Current speaker gain: 08
..OK.. Success
AT+BTRH?. Query the current "response and hold" state of the AG
..ERROR.. Error
* AT+XAPL=A-B-06. * Enable Custom AT Commands
..AT+XAPL=iPhone2.. Enable Custom AT Commands
..OK.. Success
AT+IPHONEACCEV=21921. AT+IPHONEACCEV=21921
..OK.. Success
AT+BIA=11110000. Indicators Activation
..OK.. Success
AT+CSRSF=0001000. AT+CSRSF=0001000
..+CIEV: 31.. Call Setup indicator's status report
..+CIEV: 21.. Call Status indicator's status report