Other Parts Discussed in Thread: CC2652RB
Hello,
I am using TI's LaunchPad (Ver. CC2652RB) and I would like to disable the LE secure connection and activate LE legacy pairing.
But unfortunately I am not able to implement this feature. In the configuration file of simple_central, I can only choose between [Supported,Secure only](see image 1), but in gapbondmrg.h I found the definition of unsupported secure connection(see image 2), and when I call the function GAPBondMgr_SetParameter(see image 3) to set the parameter of GAPBOND_ SECURE_CONNECTION parameter, the return value is 0x18, i.e. out of range(see image 4).
So, is it possible to close the secure connection?
Best Regards,
Yabo
1.

2.

3.

4.