This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: RSSI value measurement in simple central code

Part Number: CC2642R

Dear Team,

where i can check the RSSI value in simple central code.

my requirement is read the rssi value and stored into the another variable and transfer into the packet. 

Regards,

Shrikant K

  • Hey Shrikant,

    The out of box simple_central example contains a clock event to regularly read the RSSI of a connection. This is done by calling the HCI_ReadRssiCmd. The requirement for calling this api is that you are already in a connection, as the rssi is taken from the connection event callbacks.

    You may also be able to use the Gap_RegisterConnEventCb() API to register a callback. You'll find the rssi passed into the Gap_ConnEventRpt_t struct under lastRssi. For an example on using this API, you can check simple_peripheral.

    Hope this helps.