Other Parts Discussed in Thread: CC2541
Hello Community , A pleasant day to you. We use the following products: 1.CC2541 IC 2.IAR embedded workbench 8051 version 9.30.3 3. TI sensorTag for downloading of firmware 4.Lightblue app is used to set OAD parameters When we set the OAD parameters from the LighBlue app then we go to TI sensorTag and download the firmware to the selected IC. The time duration between the setting and performing the OAD is very less. I want to tune the duration for the above mentioned task . As per the video (refer the video name VID-iphone7s_rapidspeed)when we do the task rapidly with iPhone 7s it will execute normally. But if we do slowly it stucks in ti sensor tag app(refer the video name VID-iphone7s_slowlyupdate). if we use iPhone 6s it disconnected in Lightblue app.(refer the video name VID-iphone6s_stuck)