This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC13XX-CC26XX-SDK: key_generate.py tool for OAD is broken

Part Number: SIMPLELINK-CC13XX-CC26XX-SDK


The key_generate.py tool distributed ( simplelink_cc13xx_cc26xx_sdk_6_40_00_13\tools\common\oad\keys\key_generate.py= is broken and generates garbage with Python 2.7
It does not work with Python 3.xx on account of using tostring instead of tobytes
We managed to fix it ourselves, but it really needs to be updated to run with latest Pytholn 3.xx

  • Example garbage (actually the reverse keys looks ok)
    >"\Program Files\Python-2.7\python.exe" key_generate-does-not-work.py
    ('Private key: ', 'c5874fac013b032e0c60ec2d89926adad024c025f19f38c0cd0505e98e28ebfc')
    (' Public Key ', 'a1a3ba6b6d71b78f24ad279110aa6ead03df836bbd75aeca1163bc4d9372521ee6c47388783feabc0cbcadeced8488e1e8c829ff37fceaa9b3d8f42acf34d3b8')
    ('Public key X : ', 'a1a3ba6b6d71b78f24ad279110aa6ead03df836bbd75aeca1163bc4d9372521e')
    <type 'str'>
    a1a3ba6b6d71b78f24ad279110aa6ead03df836bbd75aeca1163bc4d9372521e
    1a 3b a6 b6 d7 1b 78 f2 4a d2 79 11 0a a6 ea d0 3d f8 36 bb d7 5a ec a1 16 3b c4 d9 37 25 21 e
    ('Public key Y: ', 'e6c47388783feabc0cbcadeced8488e1e8c829ff37fceaa9b3d8f42acf34d3b8')
    6c 47 38 87 83 fe ab c0 cb ca de ce d8 48 8e 1e 8c 82 9f f3 7f ce aa 9b 3d 8f 42 ac f3 4d 3b 8
    ('Public key X in reversed format : ', '1e5272934dbc6311caae75bd6b83df03ad6eaa109127ad248fb7716d6bbaa3a1')
    ('Public key Y in reversed format: ', 'b8d334cf2af4d8b3a9eafc37ff29c8e8e18884edecadbc0cbcea3f788873c4e6')
    ('Signer Info:', '48300f7275861fe7')
    <type 'str'>
    48 30 0f 72 75 86 1f e7

  • Hi,

    I'll take a look and get back to you tomorrow.

    Cheers,

    Marie H