Part Number: CC2564MODA
Other Parts Discussed in Thread: CC2564
Hello Ti-Team,
We started to develop a new Bluetooth product that works on a Man-in-the-middle concept. It should consist of two CC2564 modules, one configured as SINK other as SOURCE roles.
Non-assisted mode is the way to go in this project because we want to minimize delay in audio retransferring audio data from SINK to SOURCE and at the same time decode (SBC, AAC) in the SINK controller for the local audio extraction.
I ran into a problem during development and I hope you can help me.
Provided Bluetopia SDK sample applications (attachment) demonstrate both roles: "A3DP Sink Demo" and "A3DP Source Demo" in "assisted" mode.
"AUD demo (A2DP)" which works in "non-assisted" mode, and is used to transfer high-quality audio, is in the SINK role only.
My question is: Is it possible to use CC2564 in a SOURCE role, "non-assisted" mode (a demo application for this mode is unavailable)?
And if it is, is there an application showing how to implement it?
Thank you very much for your answer and best regards,
Bostjan