This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Some scanning issues.

Part Number: CC2652R
Other Parts Discussed in Thread: SYSCONFIG

Hi team,

Here's the request from the customer:

1. In cc2642 with the sdk_5_20.The multi_role project does not find the scan end event. Customer needed to set up continuous scan, but when he set the scan parameters, it could only scan for a duration and then stop scanning. He wanted to restart the scan in the stopped scan event , but there is no such event. If there is no scan end event, how can him set up a continuous scan? Suppose the scan window is 100ms, the duration is 10s, and the scan interval is 1s. The result of my current verification is that it only lasts 10s. It is a scan duration that will end, but there is no event that enters disable event after the end.


2. When he is testing low power consumption, why can’t him enter in when commenting out the initialization of the peripherals? He can only test the low power by deleting the peripheral configuration in sysconfig.

Could you help check this case? Thanks.

Best Regards,                                                       

Nick