Part Number: CC2650
Other Parts Discussed in Thread: CC2640R2F, CC2642R
Hi Experts,
Good day.
Customer is working on a research project and would like to verify a few details about acceleration measurement/capture using the sensor tag CC2650. They are working on a healthcare research project and had a few questions re: sensor tag CC2650 and the accelerometer.
[1] Does the sensor tag automatically detect frequencies of 0.5 to 80 Hz (we're referring to an ISO guideline re: accelerometer use), or do we have to intentionally set it to detect this range?
[2] In terms of vibration/acceleration data sampling frequency, there is an option in the settings to set how many data points per second are recorded/displayed. Customer chose 3 data points per second for their data collection. Does this literally mean the sensor tag only sampled 3 data points per second or were they "mean" values collected 3 times per second?
Someone has mentioned that for ISO standards we should have a data sampling of at least 50-100 points per second. Please clarify if that is recommended when using the sensor tag CC2650. Thanks
Regards,
Archie A.