Team,
Mindtree is not responding and we need help, Gluzman diverted to E2E only today putting more pressure to get an answer TOMORROW.
Here with the status:
Started development on MSPEXP-PAN13xx BT_ANT SDK (Beta 1.0)
Philips changed the interupt vector address which significantly improved the reliabilty.
When they noticed the instability they moved to : MSP430F5438 EXP Board + PAN13xx Bluetooth SDK GA 1.0
They tested the GA 1.0 version with additional SW code, see attached file (100ms wait + toggle LED) with FreeRTOS OS tick enabled.
With this addtion they experienced:
- hang-up (at different stages of the SW)
- HCI Uart seem to stop with BT communication
- application error
- Program Counter error
Can you verify and reproduce the errors Philips has with our SDK ?
We have to have an update by July 5th!!
PS: Philips noticed that for both SW versions the BT stack is binary compatible.
Let me know if you need addtional info.
Best regards,
Frank