Part Number: CC2564CMSP432BTBLESW
Hi,
all Bluetooth Low Energy examples from the CC2564CMSP432BTBLESW-v5.1.1.0-Setup.exe release do not link and the following error is shown:
error #10008-D: cannot find file "SS1BTDIS.lib"
For example, the PXP Demo tries to link all of the following libraries: -lSS1BTDIS.lib -lSS1BTGAP.lib -lSS1BTGAT.lib -lSS1BTIAS.lib -lSS1BTLLS.lib -lSS1BTTPS.lib
A quick look into my installation directory reveals that SS1BTGAP.lib lives in c:\ti\Connectivity\CC256X BT\CC256x MSP432 Bluetopia SDK\v5.1.1.0\Bluetopia\profiles\gaps\lib\ccs\SS1BTGAP.lib, SS1BTLLS.lib lives in c:\ti\Connectivity\CC256X BT\CC256x MSP432 Bluetopia SDK\v5.1.1.0\Bluetopia\profiles\lls\lib\ccs\SS1BTLLS.lib and so on, ie. always in the <profile>\lib\ccs subdirectory.
However, the dis\ directory only contains an include\ directory, but no lib\ directory where the .lib file should be present.
So the question is: Is this library missing in that release or is there something else wrong?
I tried to download an older version of the driver package to verify this, but unfortunately I could not find an older version.