Part Number: CC2652R7
Other Parts Discussed in Thread: CC3200, CC3220SF, CC3235SF, CC3135, CC2564C
Hi
I have a requirement where I have to detect the seat occupancy(Sensor node) and seat belt(Sensor Node) status notification of each seat kids seat at the bus drivers cabin device.
For the sensor node device I shall be using CC2652R7 as a BLE advertisers. The seat number as well as the status of the seat belt sensor and the occupancy sensor data of the will be be part of the advertising packet data.
Now the reason to go with CC2652R7 is because instead of regular BLE 5.2 baed advertisement I may also go for theCoded PHY (S2 and S8) based advertisement in order to extend the network area.
For the drivers cabin I want to develop the HUB which will DC powered and its role will be to scan the BLE advertisements and then send that data to a WLAN based server for storing or for viewing into the Mobile application via WLAN.
For the BLE to WLAN based gateway HUB device, I would like to have CC2652R7 for the BLE operation so that I shall have the flexibility to move to Coded PHY (S2 and S8) based scanning if my sensor node are configured for Coded PHY based advertisement as well I can switch for normal BLE5.2 based scanning when my sensor node are configured for normal BLE5.2 based advertisements.
Can anyone suggest me a suitable IC for the WIFI based Operation, I am not sure if CC3200 or CC3235 should be my choice for WIFI ?
Is there any development kit or any hardware available with Texas instrument so that I can use it for my development purpose for BLE to WIFI HUB.
Regards
Piyush Saxena