Hi,team:
Hello! I encountered the following problems when designing products using CC1352P7, an RF chip:
1. Designing a product using CC1352P7, using + 20dbm to output Sub1G band, +14dbm to receive Sub1G band, 2.4G band not used,
two RF antenna interfaces, one to transmit signals and the other to receive signals. Do you need to use no RF switch?
2. As the first question said,If no RF switch is used, when 20dbm signal is sent, the receiving channel can receive the sent signal,
will it damage the receiving channel?