This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: How can I connect it to the desktop and change the firmware?

Part Number: CC2650STK

Hi there,

I am modifying the code so that 100 sensor values ​​can be passed in 1 second in the default sdk. I am trying to compile and download to my cc2650stk board to see the result of modifying the code.

However, when I run Flash Programmer2, the computer does not recognize the sensor. I thought it was a problem with the program, so I checked it with Tera Term, but it said there was no connection value. It seems that the computer does not recognize it. What should I do?

And is it correct to use Flash programmer2 to download hex files to cc2650stk?

The dev pack lights up, but tera term and flash programmer do not recognize it. This is a picture showing it.