Part Number: CC2640R2F
hi team:
I am using the Sensor Controller Studio coprocessor for low-power design.
I want to write the corresponding configuration to the register address specified by the sensor using SPI communication,
such as writing 0x03 configuration information to the register at address 0x01 and writing 0x05 configuration information to the register at address 0x02.
I would like to know how this is achieved (can it be achieved through spiTx8bit (# cfg, txValue))?
Additionally, I noticed in your document that the SPI data transmission function only specifies the transmission method and data to be transmitted.
If I use the API multiple times, does it default to writing configuration information from the register at address 0x01?