This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: Loading CC2650 firmware into LAUNCHXL-CC2640R2

Part Number: LAUNCHXL-CC2640R2


Hi, I'm trying to use the example "simple_peripheral" of the ble_sdk_2_02_07_06 with my LAUNCHXL-CC2640R2. The reason is that it seems that this ble sdk runs with bluetooth 5.1. However, when I load the code nothing happens: the system does not advertise, when I configure LEDs they don't blink and etc. What I should I do to make the fw compatible with the board?