Background information:
- When using the pictured System #1 (TI hardware / TI firmware / TI Packet Sniffer App), the signal strength results are in dBm. These results are useful and meaningful, because they are comparable to other systems.
- When using the pictured System #2 (TI hardware / TI firmware / TI BTool app), the signal strength results are in a 0-250 unitless scale. These results are not useful or meaningful, because we can not calculate the equivalent dBm (or mW) value, so we can not compare to other systems.
- But we need to use System #2 for our test-rig (because it is easier to connect our test-rig API to the TI BTool app).
Question:
When using the pictured System #2 (TI hardware / TI firmware / TI BTool app), how do we calculate the dBm (or mW) value from the 0-250 result?