This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: Power consumption is weird

Expert 3991 points
Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5, ENERGYTRACE, SYSCONFIG

Hi Champs,

I am trying with the example project "rfPacketRx_LP_EM_CC2340R5_nortos_ticlang".

I didn't modify anything. However the EnergyTrace showed high power current consumption: >12mA without the LED.

Even when I tried to put the MCU in standby mode by using the function sleep(), the current was still >4mA. Where does this 4mA come from?

I also don't understand why there are UART, DMA and Temperature added in the SysConfig. Could anyone please advise?

Regards,

Kien Nguyen