Part Number: LP-CC2651P3
Hi,
We have the provision to set the BLE Tx Power using syscfg Tool. We want to Modify the Tx Power 0-20 dbm. We want to Test the Module Performance at 0dbm, 2dbm, 4dbm, 6dbm, 8dbm,1 0dbm, 12dbm, 14dbm, 16dbm, 18dbm, 20 dbm.
Please Let us know the Possible Ranges of Selection and

// 2400 MHz, 5 + 20 dBm
RF_TxPowerTable_Entry txPowerTable_2400_pa5_20[TXPOWERTABLE_2400_PA5_20_SIZE] =
{
{-20, RF_TxPowerTable_DEFAULT_PA_ENTRY(8, 3, 0, 2) }, // 0x04C8
{-18, RF_TxPowerTable_DEFAULT_PA_ENTRY(10, 3, 0, 2) }, // 0x04CA
{-15, RF_TxPowerTable_DEFAULT_PA_ENTRY(13, 3, 0, 3) }, // 0x06CD
{-12, RF_TxPowerTable_DEFAULT_PA_ENTRY(16, 3, 0, 5) }, // 0x0AD0
{-10, RF_TxPowerTable_DEFAULT_PA_ENTRY(19, 3, 0, 5) }, // 0x0AD3
{-9, RF_TxPowerTable_DEFAULT_PA_ENTRY(20, 3, 0, 6) }, // 0x0CD4
{-6, RF_TxPowerTable_DEFAULT_PA_ENTRY(19, 2, 0, 11) }, // 0x1693
{-5, RF_TxPowerTable_DEFAULT_PA_ENTRY(21, 2, 0, 11) }, // 0x1695
{-3, RF_TxPowerTable_DEFAULT_PA_ENTRY(25, 2, 0, 12) }, // 0x1899
{0, RF_TxPowerTable_DEFAULT_PA_ENTRY(29, 1, 0, 22) }, // 0x2C5D
{1, RF_TxPowerTable_DEFAULT_PA_ENTRY(33, 1, 0, 25) }, // 0x3261
{2, RF_TxPowerTable_DEFAULT_PA_ENTRY(38, 1, 0, 31) }, // 0x3E66
{3, RF_TxPowerTable_DEFAULT_PA_ENTRY(47, 1, 0, 36) }, // 0x486F
{4, RF_TxPowerTable_DEFAULT_PA_ENTRY(32, 0, 0, 65) }, // 0x8220
{5, RF_TxPowerTable_DEFAULT_PA_ENTRY(46, 0, 0, 59) }, // 0x762E
{14, RF_TxPowerTable_HIGH_PA_ENTRY(22, 3, 1, 19, 27) }, // 0x1B27D6
{15, RF_TxPowerTable_HIGH_PA_ENTRY(26, 3, 1, 23, 27) }, // 0x1B2FDA
{16, RF_TxPowerTable_HIGH_PA_ENTRY(30, 3, 1, 28, 27) }, // 0x1B39DE
{17, RF_TxPowerTable_HIGH_PA_ENTRY(37, 3, 1, 39, 27) }, // 0x1B4FE5
{18, RF_TxPowerTable_HIGH_PA_ENTRY(32, 3, 1, 35, 48) }, // 0x3047E0
{19, RF_TxPowerTable_HIGH_PA_ENTRY(34, 3, 1, 48, 63) }, // 0x3F61E2
{20, RF_TxPowerTable_HIGH_PA_ENTRY(53, 3, 1, 58, 63) }, // 0x3F75F5
RF_TxPowerTable_TERMINATION_ENTRY
};
if We want to use the range between 6dbm-13dbm then how to select the range using the syscfg tool. Please Let us Know.
Thanks.