Part Number: CC2652P7
Other Parts Discussed in Thread: SYSCONFIG
Hello,
If I have a CC2652P7 part running DMM BLE + Zigbee, can it also run WiFi coexistence at the same time?
Regards,
James
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello James,
This is available from the SysConfig -> RF module of the DMM project, however only one stack (BLE or IEEE 802.15.4) can be selected for WiFi Coexistence. See the Coexistence section of the BLE5-Stack User's Guide for more information.
Regards,
Ryan
Thanks Ryan,
If a user wanted to somehow have a system running BLE, Zigbee, and Wifi, what would be the best configuration to manage coexistence? How many chips would be needed?
The optimal setup is a two-chip solution which has Wi-Fi coexistence enabled separately for the BLE and Zigbee devices. If this is not possible then it depends on which stack the user prefers and it is necessary to give that stack precedence in the DMM policy scheduler and GPT so that the lesser stack does not have radio usage even though the first stack is blocked by Wi-Fi usage..
Regards,
Ryan