Part Number: LP-CC2652R7
Other Parts Discussed in Thread: CC2652R7
Hi Experts,
I am trying to add OAD Onchip (Over the air download using internal memory) to the "project_zero_LP_CC2652R7_tirtos7_ticlang" example project. Is there any documentation or example code that I can follow to implement this? I have made custom board for CC2652R7 board but not included an external flash like in launchpad, so I'm going to do onchip OAD with internal flash memory. available Project zero example gives "OAD Failed to open " error since it does not have external flash memory,
Memory allocation as follows.

SDK Version : 7.10.00.98
CCS Version : V 12
Looking forward your answers,
Thank you