This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Design help questions

Part Number: CC2652R


Hi Experts,

Posted on behalf of customer as he currently does not have valid email to use:

Still has some questions:
1. How to programming internal ROM? via UART1?
2. May I power down BLE when I don't need it?
3. Would this MCU configure as slave to be a BLE module?

Regards,
Archie A.

Ref:
https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/874253/ccs-launchxl-cc26x2r1-is-it-possible-to-establish-communication-between-multiple-i2c-masters

  • Hi,

    1. CC2652R has 256KB of ROM for protocols and library functions, it's preferable for customer to write in the flash memory

    2. Yes, this MCU can run without the BLE stack and you can stay in sleep mode if you need at any moment.

    3. Also yes, the CC2652R device supports both peripheral and central mode for Bluetooth Low Energy.

    regards,