Other Parts Discussed in Thread: CC1354P10, UNIFLASH
Hello, TI teams,
There is some issue about MCUboot on following circustoms.
SDK : simplelink_cc13xx_cc26xx_sdk_7_10_00_98
example : basic_ble_oad_onchip, basic_persistent, mcuboot (in LP_EM_CC1354P10_6)
There is different working by MCUboot.
==============================
I just built using mcuboot example and programming mcuboot image with basic_ble_oad_on_chip and basic_persistent.
But it is not working normally. (It seems that boot fail because RED LED is blinking)
So I applied mcuboot image which is in the hexfiles folder instead of built image.
It is working normally.
Why does it different working? (built mcuboot mage vs mcuboot image which is in the hexfiles folder)
Please let me know the reason why it is different.
Thanks.
Jay. Son