Hi,
I followed up the tutorials, and got to the part where I start to look at code and actually understand how things work all together, thing is, as I try to follow up the example in the Software developers guide, I see that the IAR IDE... is not what I'm used to.
So I was wondering, are there other IDEs out there except the IAR?
Since the last time I wrote in C++ was 10 years ago, and that most of the code I see is C, I'm not really sure how the IAR IDE manages its project imports, build path, etc, but do you think it would be possible to migrate the project to another IDE (Specifically Eclipse for C/C++) , and keep the project setup and functionality intact, with minor import changes? (I assume that for debugging I would have to use the IAR or could I also import the debugging drivers).
Thanks,
Adam.