This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2674R10: Time synchronization over BLE

Part Number: CC2674R10

Hello,

We are developing a system that needs to accurately synchronization clocks between 2 microcontrollers over Bluetooth LE connection. Each MCU will have one sensor connected via I2C or SPI. The time synchronization must be as accurate as possible and held over a longer time. The purpose for the requirement is that sensor readings from two mobile devices need to be taken at the same time and later processed on a PC. A first estimate of the required accuracy is < 1 ms, but this is still under discussion.

Does the TI CC2674R10 (or other?) and its BT software stack support time synchronization over Bluetooth? Is there example code or instructions on how to do this?

Best regards,

Richard van Paasen.