Hi expert,
I have some questions about the throughput of CC2650&CC2340:
- Do we have exiting image of CC2650 throughput test I can flash the device directly?
- What is the throughput of CC2340 & CC2650 in the real world, and can their throughput achieve 1Mbps in the real world?
I found some comments in E2E, is that correct for all CCxx devices which have the same PHY?
- Coded S=8: ~58kbps
- Coded S=2: ~175kbps
- 1Mbps: ~780kpbs
- 2Mbps: ~1366kpbs
- Do we have throughput test example of CC2340 in SDK? If not, what should I do to test the CC2340 throughput?
Best Regards,
Seamus