This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: MCUBoot verification has delay to start application

Part Number: CC2340R5


Hi,

     I am using basic_ble_oad_onchip and I have loaded example MCUBoot bin file, example persistent app bin file from SDK and Application code. After restart its  taking approx. 10 seconds to start the application .Application requires less than 500ms for the application to start. Is there a way to optimize the MCUBoot code to speed up the process?

SDK version : simplelink_lowpower_f3_sdk_7_10_00_35

Thanks,

vignesh.