This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BTool Version Compatibility

Hi Expert,

I want do know if I can use latest BTool version with all BLE connectivity products, or I need choose the correct one in the corresponding SDK ?

For example: Can I use BTool (v1.44.02 BLE5) in simplelink_lowpower_f3_sdk_7_20_00_29\tools\ble5stack\btool with CC1352 or CC2652 launchpads?

Best Regards,

Seamus

  • Hi Seamus,

    Yes, you can use BTool (v1.44.02 BLE5) in simplelink_lowpower_f3_sdk_7_20_00_29\tools\ble5stack\btool with CC1352 or CC2652 launchpads.

    In general, the only issue you may find is that certain Vendor Specific commands are not available on all the devices i.e. may not be available in the BTool version you are using.

    Best regards,