Part Number: CC2674R10
Other Parts Discussed in Thread: ENERGYTRACE,
Customer using LP-EM-CC1354P10-1 to evaluate CC2652R10. They now have the LP running Project Zero with a 2,000msec advertising interval. EnergyTrace says the mean current draw is 1.75mA which is definitely too high for their application (target below 0.3 mA average). They understand project zero is probably not ideal use case for Low Power.
Any guidance on BLE peripheral projects that can be use to benchmark this power performance? It needs to be sending connectable advertisements.