Part Number: CC2642R-Q1
Hi Engineers
I'm facing a 100% reproducible issue when using UART driver in SDK 5.20
1. use a external MCU to transmit a particular packet to 2642 via UART
2. 2642 will UART_close after receiving this packet
3. MCU will wait for 2s then pull low RX of UART of 2642
4. 2642 will open UART again and toggle via UART TX to MCU
5. after receiving this toggle, MCU will pull high RX of UART of 2642
6. then repeat step1-2. we can see that UART_close is not entered, register show that UART is still busy transmitting data.
could you share some insight what may cause this issue?