I have a query about the PAN132x/CC256x modules. I want to use a Stellaris Cortex M3 based device in a project and am trying to select a bluetooth module. I have seen the PAN131xETU / Stellaris DK-LM3S9B96 kit and was wondering if the 1327 and 1329 modules, when available, will also work with the same tools and hardware, as ultimately I would like a Bluetooth 2.1/Bluetooth LE/ ANT module for this project. I would like to use IAR for the development as I am familiar with it from the MSP430 dev.