Part Number: CC2640R2F
Other Parts Discussed in Thread: UNIFLASH






Hi,
I designed my custom board with 2.7 x 2.7 mm WCSP CC2640R2. I followed the steps on document that is Creating Custom board. Here is the link https://dev.ti.com/tirex/content/simplelink_cc2640r2_sdk_5_30_00_03/docs/blestack/ble_user_guide/html/ble-stack-3.x/custom-hardware.html
I created a project zero from resource explorer then followed what Markel RobregadoMarkel Robregado answered on the other similar questions. I added the necessary files to Startup folder, adjusted include options etc. But only thing that I am not sure on is configuring the RF Front-End for Custom Hardware section. Actually, I have not understand what I need to change on that section. Could you please explain that section more clear ?
I flashed my code into my custom board succesfully. When I open the Simplelink Connect application on my mobile phone, project zero R2 is shown but when I try to connect, it tries to connect for 3-5 seconds and peripheral connection timeout error is shown. In short my mobile phone see the board but cannot get signal back. Signal power is around -75 and -90 dB. I am not sure whether it is caused from configuring the RF Front-End for Custom Hardware section or my PCB design. I attached the screenshot of the error message on my mobile phone.
I also attached the some screenshot what I changed.
I am using sdk_5.30 and CCS 12.3.0
Regards,














no problem about them. Only problem left is how to configure the Board_ADC0 to be DIO_11. I can read the ADC value on my mobile phone and expressions sections on CCS. But they seems like floating value not on the DIO_11.

Hi 

e phone ( no advertisement). I attached the screenshot. I connected 3V3, GND, RESET, TMS and TCK as always from the Launchpad. Is there any other device needed or just Launchpad is enough for to flash from SmartRF Flash Programmer 2.