This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: cc2640r2f simple_observer example error lib_linker.cmd

Part Number: CC2640R2F

I am currently trying to use a simple observer sample, but when I try to build, I get the following error

[Su007]: Unable to open the command file "C:\ti\simplelink_cc2640r2_sdk_1_50_00_58\examples\rtos\CC2640R2_LAUNCHXL\blestack\simple_observer\tirtos\iar\app\..\config\lib_linker.cmd" C:\Users\kty\AppData\Local\Temp\EW12A5.tmp 1

Error while running Linker

SDK simplelink_cc2640r2_sdk_5_30_00_03 for this issue

I tried installing simplelink_cc2640r2_sdk_1_50_00_58 but it is the same

How can you copy the lib_linker.cmd file to fix the error result in a function error related to GAP.

How do I set up simple_observer to use it?

I am using IAR.