This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: CC2340R5

Part Number: CC2340R5

How to make work CC2340R5 with external power supply without Using the LP-EM debug connector after programming downloaded. 

  • Hello Manjunatha GN, 

    In order for the CC2340R5 to work with external power please connect PWR and Ground (3.3 V + GND). Do you still want to be able to debug in this configuration? Here is a snippet, CC2340R5 LaunchPad (ti.com)

    "Power supply requirements:

    The LaunchPad is designed to be powered from the LaunchPad EM Debug Probe via the LP-EM Debug connector, or from an external power supply connected to the GND and both 5V & 3V3 pin headers. When powering from the LaunchPad EM Debug Probe, the device supply voltage is fixed in 3.3 V. When powering externally, care must be taken to keep the board voltage within its operating range (1.8 V to 3.6 V). "

    Thanks,
    Alex F