Part Number: LAUNCHXL-CC26X2R1
Hi everyone,
I was trying update my new firmware/ application using OAD through SimpleLink Connect mobile app but it was not successfull due an error/alert bad TLV Magic.
I am trying to send new firmware/ application (.bin file ) using OAD through through SimpleLink connect app in mobile but while sending the new image through OAD using SimpleLink connect app, some error/alert is coming name saying :-
bad TLV Magic.
steps which i I followed while performing OAD :-
1) First I flashed all 3 file which are required to perform OAD, BIM(hex), Persistent (.bin) , and simple_peripheral_oad_on_chip(.bin) into controller. (it was successfully flashed).
2)after than I made changes in multi_role project and made it OAD features enable by following Bluetooth Low Energy Enhanced Over the Air Download (OAD) Advanced — CC13XX CC26XX SimpleLink Academy (ti.com) and i was able do OAD using BTOOL , it was successful.
3)Than I tried to send image .bin file of simple_peripheral_oad_on_chip through SimpleLink connect (clicked on FW update ) but failed to do so due some error I have attached the screenshot.
I am using :-
1) SDK version :- 7.10.01.24
2) CCS version :- 12.5.0.00007 , TI Clang v3.2.0.LTS
3)android version :- 13
4) controller :- CC2642R1F
Do you have an idea, i have also attached screenshot of it please have a look.
Thanks & Regards,
Sandeep