This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: CC2642 IAR Error

Part Number: CC2642R

Hi

I'm using simplelink_cc13xx_cc26xx_sdk_7_10_01_24 version of the SDK, and I open the project of simple_peripheral_oad_onchip with IAR 8.50.9, and it reports an error what is the reason for this

  • Hi,

    I am afraid you are not using the recommend version of IAR for this SDK. You should use EWARM-9.32.1 as mentioned in the SDK release notes.

    I would recommend installing the recommended version of IAR.

    In case this is not possible, you may want to try to convert this "diagnostic tag  pa205 does not exist" error to a warning (see here) to see if you manage to pass the compilation stage. However, please remember the SDK is not tested for the IAR version you are using which may lead to unexpected behaviors.

    I hope this will help,

    Best regards,