Hi,
I wanted to try the "Simple-Application" on the MSP-EXP430F5438. I downloaded the MSPEXP-PAN13xx SDK from TI and installed the PAN1315ETU on the Experimenter's Board as described in the Developer's Guide including shorting the RF3 pins.
I'm using the IAR Workbench 30-day Evaluation version with an Olimex for debugging. After downloading the application onto the Experimenter's Board and clicking on "Go", the programm gets stuck during the BT_UART_ISR (msp430_uart.c ) in the line UART_TRANSMIT(buff_data);
Everytime I break I get the following warning: The stack pointer for stack 'Stack' (currently Memory:0x293C) is outside the stack range (Memory:0x5B60 to Memory:0x5C00)
I honestly don't know where to start looking for the problem, if it's because of something on the Experimenter's Board like a jumper connection I forgot or if it's some configuration of the IAR workbench.
I also have one other question concerning the IAR workbench: For my own application I copied the "Simple Application" into a empty project and changed it in a few places and now the IAR workbench downloads the application but afterward I can't go through the application as "Go", "Step into" etc are disabled and the first line of my main-function isn't highlighted green.
Can someone help me with those 2 problems?
Lizzy