This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: BT

Part Number: CC2640

We had a requirement where the TI bt chip CC2640 needed to be controlled from the host CPU and the TI bt chip CC2640 needed to act both as a peripheral and central, based on the need. While trying out, we figured out that running "Host Test sample application" on CC2640 and develop an application code which will use HCI commands like "btool" is the best way to go about it. While we know that "btool" is not an open source tool. So we were wondering if there place where the HCI/GAP/GAAT source code is available so that we can leverage the same to write our application which will control the CC2640 from host CPU just like btool. 

Regards,

Sumanth N