Part Number: CC2642R
HI,
CC2642 do host to connect CC2642 slave, establish a connection after a delay of 30 seconds after the host initiative request to disconnect, but pressure test 1 day 2 ~ 3 times after the host send disconnect request slave did not reply, the slave directly disconnected, the host after 3 seconds before 0x08 timeout disconnect.
Test distance: <50cm
sdk version: simplelink_cc13xx_cc26xx_sdk_7_10_01_24
Project example: multi_role

The first disconnect command sent by the master, the slave rebroadcasts the