Part Number: WL1831MOD
I am trying to get the WL1831MOD to work with my zynq device.
I can see CTS and RTS going low, and using the bluetooth logger tool I can also see both devices communicating over the HCI interface. However I get the following error in my dmesg, and "hciconfig hci0 up" will timeout.
Bluetooth: hci0: command 0xfd06 tx timeout hrtimer: interrupt took 19933 ns Bluetooth: hci0: send command failed Bluetooth: hci0: download firmware failed, retrying... Bluetooth: hci0: command 0x1001 tx timeout Bluetooth: hci0: Reading TI version information failed (-110) Bluetooth: hci0: download firmware failed, retrying... Bluetooth: hci0: command 0x1001 tx timeout Bluetooth: hci0: Reading TI version information failed (-110) Bluetooth: hci0: download firmware failed, retrying... Bluetooth: hci0: command 0x1001 tx timeout
Do you have any idea what could be causing this issue? I can give you the bluetooth log if that can help.
Thanks,
Alex