Hi Ti Experts.
I need to make a central role to connect peripherals.
I have completed Scan and connect.
Next, when I wanted to discover services, he did not respond to any events.
void Central_disc_start() { uint8_t uuid[ATT_BT_UUID_SIZE] = { gServiceUUID[1],gServiceUUID[0]}; // Initialize service discovery variables svcStartHdl = svcEndHdl = charHdl = 0; // Discover service by UUID //bStatus_t status = GATT_DiscPrimaryServiceByUUID(Connection_getConnhandle(0), uuid, // ATT_BT_UUID_SIZE, ICall_getEntityId()); bStatus_t status = GATT_DiscAllPrimaryServices(Connection_getConnhandle(0),/*ICall_getEntityId()*/INVALID_TASK_ID); PRINT_DATA("[weli]%s-%d,status:%d\r\n",__FUNCTION__,__LINE__,status); }
the log as below.
[weli]Central_disc_start-568,status:0
But when I change INVALID_TASK_ID to ICall_getEntityId(), the GATT_EventHandler will return event:4 when I call Central_disc_start.
static void GATT_EventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData) { PRINT_DATA("[weli]%s-%d:event:%d\r\n",__FUNCTION__,__LINE__,event); //response event:4 gattMsgEvent_t *gattMsg = ( gattMsgEvent_t * )pMsgData; switch ( gattMsg->method ) { case ATT_FLOW_CTRL_VIOLATED_EVENT: { MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE, 0, "GATT status: ATT flow control is violated"); } break; case ATT_MTU_UPDATED_EVENT: { MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE, 0, "GATT status: ATT MTU update to %d", (( attMtuUpdatedEvt_t * )pMsgData)->MTU); } break; default: break; } }
In addition, I have set Gatt's event mask to 0xffff,
BLEAppUtil_EventHandler_t dataGATTHandler = { .handlerType = BLEAPPUTIL_GATT_TYPE, .pEventHandler = GATT_EventHandler, .eventMask = 0xffff//BLEAPPUTIL_ATT_FLOW_CTRL_VIOLATED_EVENT | //BLEAPPUTIL_ATT_MTU_UPDATED_EVENT };
Please tell me if I missed anything.
Also, are there any tutorials on discovering service notify characteristics?
Thanks.