Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG,
When using the Basic BLE example, if I use sysconfig to switch from "Connectable and scanable undirected" to "Non-Connectable and non-scanable undirected" the advertisements are gone when I run the sample. It is printing out the MAC address so I know what to look for, I get a single packet and then nothing. Is that correct behavior? I thought it would keep advertising at the 100ms interval in the example.
Note you have to use Peripheral mode, switching to Broadcast mode causes a sysconfig error.