Part Number: CC2540
Hi, FAE team,
We have problem in generating hex file using the tool of " SmartRF Flash Programmer ". we did succeed in the procedure in about 2020. but now we have problem although the procedure is same and we are familiar with it.
The failed procedure is as following.
- A test.bin was download to a PCB1, it worked, Everything was OK.
- Use TI's software tool to read and save the data from the flash of PCB1 as a .hex file, named as test.hex
- Erased the program on PCB2 using TI's software tool. Use the newly generated test.hex file. checked the option box of "Erase, program and verify". After programming and verification, PCB2 didn't not work normally as expected
- Repeated the same procedure for PCB1, the text.hex worked for PCB1.
In a word, now the hex files can work only in the PCB1 on which it was generated. but not for other pcbs.
We used 2540 for years and the last application bin file was released in 2020 and the generated hex file worked well. However, when we upgrade the firmware and want to repeat the procedure to get hex file from bin file now. It doesn't work. We don't know why. How do we fix this problem? .
Thanks.