I've got two CC2540 USB dongles and one Keyfob. One USB dongle has the HostTestRelease firmware and the other has the packet sniffer loaded. The Keyfob has the KeyFobDemo loaded. I use BTool to connect to the Keyfob. With the packetsniffer I'm looking at the RSSI of the packets sent from the dongle. Now I use BTool to change the Tx power level using the HCIExt_SetTxPower command. The command completes successful, but I can not ever notice any difference in RSSI on the packet sniffer. I expect that I would see a big difference of the RSSI if I switch form +4dB to -23dB.
For this test I used all the original software without any modification as it comes with the BLE 1.1 release. Any ideas what might be wrong?