Hi ,
We are using the The simplelink_lowpower_f3_sdk_7_40_00_64 , which provides the basic ble example which is written using FreeRTOS.
Question #1:
Does the TI provided FreeRTOS based application can be taken as reference and develop our production firmware.
In that case do we need to procure FreeRTOS license separately or the license TI got for using FreeRTOS can be leveraged.
Question#2:
Do we have non RTOS based sample BLE application such that we can avoid using RTOS based firmware application.
Also please suggest if there are any other alternate method.
With Regards
Ilanchezhian T