Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: CC2642R-Q1
I am trying to flash CC2642R-Q1 in Backdoor boot loader mode via SPI.
After reset, the chip is responding to PING command after 5s. Is that expected?
And if i continuously send commands in 100ms loop there is a delay in getting response(taking 2 to 3 sec for each command).
(For ex: CRC32 command responding after 3s with 7 retries)
How to solve the delay in response?
Is there any specific baud rate for SPI communication?