Other Parts Discussed in Thread: CC2640, UNIFLASH
Hi, I am working with RF Star module based on CC2640R2FRSMR, integrated on my custom board for a BLE application.
I am also using BQ24078 for Power Management on my board.
In order to upload the code I am using CC2640 Launchpad with its VCC, GND, RST, TMS, TCK pins as JTAG.
I am able to connect to, as well as transmit data from my board when in the debug mode in CCS, however when I switch to battery by disconnecting the JTAG, I momentarily see the advertisement of my custom board but it disappears after about a second and therefore I am not able to connect to it via BLE.
Note: I am able to see a 3.7V level at the VCC of the RF star module, when battery is connected.
Also, when I connect the battery and simultaneously put the board in Debug mode, i am able to transmit data. At this point when I disconnect the JTAG, the device still works. Now when I upload the code on the board and completely switch to battery (ie, no JTAG this time), even though the VCC receives 3.7V, I am not able to see any advertisement.
Can you pls suggest what could be wrong?
On the left side, RST and GND are 2 of the 5 pins of JTAG, and on the right side, RST is connected to the reset pin of the module.
Please let me know if any other info is required.
Regards,
Ritoo