Hello,
I'm interested in implementing large RF network, built of up to 1024 sensors, each of them have to send 10 octets of new information every 10 minutes. This information should reach the data concentration station in reasonable time (up to 5 minutes).
The problem is that these sensors are moving in a wide area, and i assume that every 10-20 seconds, 5% of currently established pairs may break and appear differently, therefore this MESH structure is moderately dinamic in nature.
Because of the size of area in which these sensors may move, practical ISM RF implementation leads to 8 hops between the MESH edges and even more.
Can anyone advise if this is feasible with ANT? What average network latency should be expected in such case? Power consumption issues?
Thanx in advance,
Eli.